Changing Saturation Times - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
If you are building the application, follow these steps:
  1. Disconnect the connection between the saturation output on the PID Pre-Processor and the saturation time input on the PID.
  2. Give the PID's saturation time input a default value of the desired saturation time.
If you are working on a running Metasys system, follow these steps:
  1. Note the outputs of the PID Pre-Processor.
  2. Change the default value on the inputs to the PID Pre-Processor to match the original outputs.
  3. Change the Saturation Time input's default value on the PID Pre-Processor to the desired value.
  4. Set standard tuning to false on the PID Pre-Processor.