Adding a Trend in an Advanced Application Controller - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Start CCT/PCT and open the controller application.
  2. Click the Advanced tab in the lower section of the screen. The Advanced tab tree and information screen appears.
    Note: If necessary, resize the screen for a better view of the Advanced tab information.
  3. Right-click Trends and click Add Trend.
  4. Click the Trend you added and click Edit. The fields you can edit appear in white.
  5. Click the button next to the Input Reference field and click the point you want to trend.
  6. Click OK.
  7. Enter the remaining trend parameters. Refer to the Trend Screen section in the Controller Tool Help (LIT-12011147) for more information on field parameters.
  8. Click Apply.

Results

Note: To add trends to objects in a supervisory controller, refer to the Trend Extensions section in Metasys System Help (LIT-1201793).