Process IDs - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Characteristics that are common to numerous standard control loops are grouped together into process IDs. The process ID sets the initial tuning parameters and the expected time constant for the control loop. The initial system parameters include dead time, process range, and time constant. Prior to Release 5.1, or in certain upgrades where the PID pre-processor is not connected to the PID inputs of interval, proportional band, integral time, and saturation time, the following equations determine the initial values of proportional band and integral time from the values for dead time, process range, and time constant. At Release 5.1 and later, the proportional band and integral time values are determined by what is on their inputs.



Note: Time constant is represented by , process dead time is represented by , and process range is abbreviated as PR.

In addition, the parameters of dead time, process range, and time constant also determine saturation time, interval (period), and minimum tune band. These parameters remain constant and are unchanged by PRAC+ adaptive tuning. Therefore, make sure to select the correct process ID for the mechanical system.

CCT/PCT process IDs and associated standard tuning parameters have been selected based on typical mechanical system design criteria. When a mechanical system's design and performance is different from what was considered typical when the CCT/PCT standards were created, the PRAC+ adaptive tuning may not perform as expected. Sometimes the system can benefit from changing the process ID to a different ID that is more representative of the system. For example, a lab or operating room with a high air change rate may more closely resemble a wide space in a duct than it does a room, and may benefit from changing the process ID from Zone Temperature (ZN-T) to Discharge Air Temperature (DA-T). When you compare the performance characteristics defined by these two process IDs in Table 1, you can see that the DA-T is much quicker to detect changes (shorter dead time) and to detect most of the change much quicker (time constant). As a result, the values for saturation time and period are much shorter.
Table 1. Comparison of Process IDs

Parameter

ZN-T (°F)

DA-T (°F)

Dead Time

30

20

Process Range

27

54

Time Constant

900

200

Saturation Time

300

60

Interval (Period)

60

12

Minimum Tune Band (PR x 0.04)

1.08

2.16

At Metasys Release 5.1, several process IDs were changed to be much more aggressive. If you transfer an application to the computer, upgrade, and then transfer the application to the device, the control continues with the tuning parameters at the time of the transfer to computer. If you use an application that was created in CCT/PCT and still has the default tuning parameters, and you upgrade to CCT/PCT 5.1 or later, the control uses the more aggressive tuning parameters introduced at Release 5.1. See Appendix: Process IDs for the initial values of process IDs across recent Metasys releases.