PRAC Status Output - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
The PRAC Status Output displays details about what the PRAC+ calculation did during its most recent execution. You can view the PRAC Status Output in the Simulate mode or the Commission mode of the CCT/PCT UI. Right-click the PID and select View > Details (Figure 1). Table 1 provides a brief overview of the messages that appear in the PRAC Status Output.
Figure 1. PRAC Status Output

Table 1. PRAC Status Output Values

Message

Description

Normal

Operation is normal.

Monitoring load disturbance

PRAC is monitoring the pattern of a load disturbance.

Monitoring setpoint change

PRAC is monitoring the pattern of a setpoint change.

Tuning not updated

PRAC monitored a pattern of a load disturbance or setpoint change and determined the pattern to be insignificant.

Gain decreased

The proportional band was increased due to an aggressive or unstable control.

Gain increased

The proportional band was decreased due to a slow oscillation

Normal tuning update

PRAC has monitored a pattern and performed an update of the proportional band and integral time.