Output Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The outputs module category lists the outputs defined for the system. Outputs are the points that get connected to an actual device, representing a physical hardware point in the system. Outputs can also represent a point associated with an output. Outputs send data to hardware output points of a device. Outputs may be connected to the Network Sensor, as well as Analog Inputs, Analog Outputs, Binary Inputs, and Binary Outputs.

See the following sections for information:

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.