Primary States (Sideloop Reset Output) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Min: The Present Value is set to Output Range Low.

  • Max: The Present Value is set to Output Range High.

  • Control: The Input is spanned using the Input Range Low, Input Range High, Output Range Low, and Output Range High to produce the Present Value.