Sideloop Interlock Binary to Binary - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module passes the enumerated value (typically from a Binary Input) to an enumerated output (typically connect to a Binary Output). The value may be delayed based on the selected delay type (None, On, Off, or Both.)

You can view and modify the modules in this group’s logic.

The Sideloop Interlock Binary to Binary modules work with the state selection mode (optional).

To see a module's connections and how modules interact with it, view the Connections table.