Sideloop Interlock Binary to Analog - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module selects the value sent to a proportional output based on the enumerated input value (typically from a Binary Input). The value may be delayed based on the selected delay type (none, on, off, or both.)

You can view and modify the modules in this group’s logic.

The Sideloop Interlock Binary to Analog modules work with the state selection mode (optional).

To see a module's connections and how modules interact with it, view the Connections table.