Primary States (Sideloop Interlock Binary to Analog) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Off: The Present Value is set to Output Range Low.

  • On: The Present Value is set to Output Range High.

  • Control: If the Input is On and all timers are satisfied, the Output Range High is passed to the Present Value. If the input is Off and all timers are satisfied, the Output Range Low is passed to the Present Value.