The following table describes the attributes used by the Sideloop Binary Control module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Direct Acting |
Determines if the output controller should have a direct or reverse impact on the process variable. |
False |
|
|
Mode |
Provides the command that enables the process to run. |
Off Set Name: Off/On/Control |
|
|
Output |
Provides the output for the BO being controlled. |
Off Set Name: Off/On |
|
|
Process Variable |
Indicates the variable that is compared to the set point and is used to determine whether to turn the BO on or off. |
20 °C, 72 °F |
|
|
Setpoint |
Indicates the target value of the process variable. |
20 °C, 72 °F |
|
|
SL-Diff |
Indicates the Off/On differential. |
1 °C, 2 °F |
|
|
SL-Outstate |
Indicates the operating mode of the module. |
Normal Set Name: Control Status |