Attributes (Sideloop Binary Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Sideloop Binary Control module.

Table 1. Sideloop Binary Control Attributes

Name

Type 1

Description

Default Value

Direct Acting

 

Determines if the output controller should have a direct or reverse impact on the process variable.

False

Mode

 

Provides the command that enables the process to run.

Off

Set Name: Off/On/Control

Output

 

Provides the output for the BO being controlled.

Off

Set Name: Off/On

Process Variable

 

Indicates the variable that is compared to the set point and is used to determine whether to turn the BO on or off.

20 °C, 72 °F

Setpoint

 

Indicates the target value of the process variable.

20 °C, 72 °F

SL-Diff

 

Indicates the Off/On differential.

1 °C, 2 °F

SL-Outstate

 

Indicates the operating mode of the module.

Normal

Set Name: Control Status

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)