Sideloop - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These modules provide several methods of controlling outputs. These include simple interlocks (where the input is binary), reset control (where an analog input is spanned to produce an output), PI proportional and staged control, and PI with reset proportional and staged.