The application System Selection trees use the individual modules in this group using the names in the following table.
|
Module Instance Name |
Applications |
|---|---|
|
MSC 2 Position 2 Pipe |
|
|
MSC 2 Position Box Heating |
|
|
MSC 2 Position Cooling |
|
|
MSC 2 Position Heating |
|
|
MSC 2 Position Supplemental Heating |
|
|
MSC Staged Box Heating XX (Where XX Is 01-03) |
|
|
MSC Staged Compressor X (Where X Is 1 or 2) |
|
|
MSC Staged Cooling XX (Where XX Is 01-08) |
|
|
MSC Staged Heating XX (Where XX Is 01- 03) |
|
|
MSC Staged Humidification XX (Where XX Is 01-04) |
|
|
MSC Staged Preheat XX (Where XX Is 01-08) |
AHU Mixed Air Single Duct Applications AHU Mixed Air Dual Duct Applications AHU 100% Outdoor Air Single Duct Applications |
|
MSC Staged Reheat XX (Where XX Is 01-08) |
|
|
MSC Staged Supplemental Heating |
|
|
Sideloop MSC XX (Where XX Is 01-08) |
|
|
Zone X MSC 2 Position Heating (Where X Is 1-8) |
|
|
Zone X MSC Staged Heating XX (Where X Is 1-8 and XX Is 01-03) |
To see a module's connections and how modules interact with it, view the Connections table.