The key states are described below. If the Heating Mode is Water Flush or Shutdown, the Heating Percent Cmd is set to the Flush Position or 0%, and the state is not allowed to enter Control Heating. Otherwise, the Cooling Mode is Control and the Zone Temperature is reliable. A two-state FSM determines whether heating or cooling should be active.
Cooling Mode
-
Control: Modulates the zone damper to control the Process Variable at the Effective Setpoint. If the Process Variable is unreliable, the Damper Percent Cmd is set is based on the Unreliable output input.
-
Shutdown: Sets the Damper Percent Cmd based on the Shutdown Option input. If the input PID Tuning Reset is Normal, the Reset Tuning input to the PID is set to true causing the PID to recalculate its tuning parameters.
Heating Mode
-
Control: Modulates the heating valve to control the Process Variable at the Effective Setpoint. If the Process Variable is unreliable, the Heating Percent Cmd is set to true based on the Unreliable Option input. If the input PID Tuning Reset is not Normal, the Reset Tuning input to the PID is set to true causing the PID to recalculate its tuning parameters.
-
Shutdown: Sets the Heating Percent Cmd based on the Shutdown Option input.
-
Water Flush: Sets the Heating Percent Cmd to Flush Position. The zone damper continues to respond appropriately for heating or cooling.
|
Cooling Mode |
Heating Mode |
Shutdown Option |
Unreliable Option |
ZN-T Reliable |
FSM State |
PID Tuning Reset |
State |
|---|---|---|---|---|---|---|---|
|
Hold |
* |
* |
* |
* |
* |
Reset 1st PID |
Control Cooling |
|
Hold |
* |
* |
* |
* |
* |
Reset 2nd PID |
Control Heating |
|
Hold |
* |
* |
* |
* |
* |
* |
Hold |
|
* |
Hold |
* |
* |
* |
* |
Reset 1st PID |
Control Heating |
|
* |
Hold |
* |
* |
* |
* |
Reset 2nd PID |
Control Cooling |
|
* |
Hold |
* |
* |
* |
* |
* |
Hold |
|
Shutdown |
Not (Control) |
Open (Cooling) |
* |
* |
* |
* |
Open (Cooling) |
|
Close (Heating) |
* |
* |
* |
* |
Close (Heating) |
||
|
Hold Damper |
* |
* |
* |
* |
Hold Damper |
||
|
Control |
* |
* |
TRUE |
* |
* |
Control Heating |
|
|
Open (Cooling) |
FALSE |
* |
* |
Open (Cooling) |
|||
|
Close (Heating) |
* |
* |
Close (Heating) |
||||
|
Hold Damper |
* |
* |
Hold Damper |
||||
|
Not (Shutdown) |
* |
* |
* |
TRUE |
Cooling |
* |
Control Cooling |
|
Heating |
* |
Control Heating |
|||||
|
Open (Cooling) |
FALSE |
* |
* |
Open (Cooling) |
|||
|
Close (Heating) |
* |
* |
Close (Heating) |
||||
|
Hold Damper |
* |
* |
Hold Damper |