Module Use in Applications (Zone Damper w Proportional Heating Valve) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Zone Damper w Proportional Heating Valve Uses in Application System Selection Trees

Module Instance Name

Applications

Zone X with Proportional Heating Valve Control v51 (Where X Is 1-8)

AHU Multizone (Mixed Air Dual Duct) Applications

To see a module's connections and how modules interact with it, view the Connections table.