Multizone Zone Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Multizone Zone Control modules provide temperature control for one zone served by a constant volume, dual duct AHU. Typically the damper for the hot deck and cold deck are mechanically linked. For example, when the damper is open to one deck, the damper to the other deck is closed. These linked dampers are modulated to maintain a Zone Temperature setpoint. Some of the modules optionally sequence the dampers with control of a reheat coil. The multizone application supports up to eight independent zones, with the zone number designated by X (representing zones 1-8).