Blocking Protection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Motor Protection module monitors the output command for a motor. If the command is off for an extended period of time, the motor starts for a short amount of time.

You can view or modify the modules in this group’s logic.