The following table describes the attributes used by the Preheat Proportional Valve with Return Water Control modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Compensator Preheat Cmd |
Controls the preheat valve. The valve is commanded from 0% to 100%. This output incorporates the Lead Compensator. |
0.0 Display Units: % |
|
|
Failsoft Value |
Defines the proportional valve position or the face and bypass damper position when the module is in the Failsoft state. |
100.0% |
|
|
Flush Position |
Defines the proportional valve position when the module is in the Water Flush state. |
100.0% |
|
|
Heating Control Status |
V |
PID status. |
Normal Set Name: Control Status |
|
Heating Ramp Rate |
Determines the time to remain in the Cold Start state (if applicable). During the cold start state, the preheat output is prevented from closing quickly to allow it to come into control without tripping the Low Limit on the unit. |
20 Change per Minute |
|
|
HTG-O, PH-O, or RH-O (Heating Percent Cmd) |
V |
Controls the heating valve. The valve is commanded from 0% to 100%. |
0.0% |
|
HTG-OUTSTATE, PH-OUTSTATE, or RH-OUTSTATE (State) |
G, V |
Current operational mode of the output controller. |
Off Set Name: AHU Htg Valve State |
|
Limited Max Value |
Defines the proportional valve position when the module is in the Limited Max mode. |
100.0% |
|
|
Low Limit Process Variable |
Contains the low limit temperature process variable. This input is usually the mixed air temperature or the preheat air temperature. |
7 °C, 45 °F |
|
|
Low Limit Proportional Band |
Contains the range across which the valve is proportionally modulated open as the Low Limit Process Variable drops below the Low Limit Setpoint plus the Low Limit Proportional Band. This input is used only in the Remain In Control mode. |
5 °C, 9 °F |
|
|
Low Limit Setpoint |
Contains the low limit temperature setpoint. |
7 °C, 45 °F |
|
|
Low OA Temperature Diff |
Contains the differential for the Low OA Temperature function. When the valve is open in the Low OA Temperature Mode, the protect temperature must increase the Low OA Temperature by more than the Protect setpoint before the valve closes. |
0.5 °C, 1 °F |
|
|
Low OA Temperature Position |
Defines the proportional valve position or the face and bypass damper position when the module is in the Low OA Temperature state. |
100.0% |
|
|
Low OA Temperature Setpoint |
Contains the setpoint for the Low OA Temperature function. When the protect temperature is below this setpoint, the valve opens to the Low OA Temperature Position. |
4 °C, 40 °F |
|
|
Mode |
Mode of operation. |
Off Set Name: AHU Htg Valve Out |
|
|
OA Temperature |
Contains the outdoor air temperature. |
4 °C, 40 °F |
|
|
Output Overridden |
Indicates when the actual output controlled by this output is overridden by a user. |
False |
|
|
Output Position |
Provides the current Present Value of the output that this controller drives. |
0% |
|
|
PID Tuning Reset |
Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID. |
Normal Set Name: PID Tuning Reset |
|
|
Process ID |
Type of process that this output controller is controlling when the mode is T Control. |
DA-T Set Name: Process ID |
|
|
Process Units |
Specifies the units for the PID. For this particular module, °C and °F are the only two valid values. |
°C, °F Set Name: Unit |
|
|
Process Variable |
Control temperature. Either zone temperature, discharge air temperature, return air temperature or preheat temperature may be connected to this input. |
13 °C, 55 °F |
|
|
Pump OnOff |
Controls the circulating pump. |
Off Set Name: Off/On |
|
|
Setpoint |
Contains the desired setpoint for the process variable to be controlled to when the mode is T Control. |
13 °C, 55 °F |