-
Off: Turn everything off. The Heating Percent Cmd is set to 0%. The MSC module observes any minimum on time.
-
Max: The Heating Percent Cmd is set to 100%.
-
Limited Max: The Heating Percent Cmd is set to the Limited Max Value. This state may be used for unoccupied heating.
-
Hold: Hold the outputs at their current position.
-
Instant Shutdown: Turn everything off. The Heating Percent Cmd is set to 0%. The MSC module does not observe any minimum on time.
-
T Control: Use the heating device to control the Process Variable. The module controls the output in order to maintain the Process Variable at the Setpoint. The Heating Percent Cmd adjusts between 0% and 100%.
-
LL-T Control: Use the heating device to control the Limit Variable. The module controls the output to maintain the Limit Variable at the Limit Setpoint. The Heating Percent Cmd adjusts between 0% and 100%.
-
Low OA Temperature Startup: This mode activates the T Control state section, but limits the rate at which the valve can close so that the unit can safely come into control (typically used for 100% OA units with low OA temperatures at startup).
|
Proof of Airflow |
Mode |
PID Tuning Reset |
State |
|---|---|---|---|
|
Fault |
* |
* |
Instant Shutdown |
|
Not (Fault) |
Instant Shutdown |
* |
Instant Shutdown |
|
Off |
* |
Off |
|
|
Max |
* |
Max |
|
|
Hold |
Reset 1st PID |
T Control |
|
|
Hold |
Reset 2nd PID |
LL-T Control |
|
|
Hold |
* |
Hold |
|
|
LL-T Control |
* |
LL-T Control |
|
|
T Control |
* |
T Control |
|
|
Limited Max |
* |
Limited Max |
|
|
Low OA Temperature Startup |
* |
T Control |