Module Use in Applications (Heating Proportional Valve) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heating Proportional Valve Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Box Heating Control v51

VAV Single Duct Applications

Proportional Heating Control v51

Fan Coil Application

Proportional Supplemental Heating Control v51

VAV Single Duct Applications VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.