|
Input |
Behavior When Input Is Not Reliable |
|---|---|
|
OA Temperature |
If the requested mode is Low OA Temperature, the output controller changes to Failsoft Valve. |
|
Low Limit Process Variable |
If the requested mode is Remain In Control, the output controller changes to Failsoft Valve. |