Reliability (Cooling Proportional Valve with Dehumidification) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

All inputs use their last reliable value while unreliable.

If the outdoor air temperature is unreliable while in the Low OA Temperature mode, the module switches to the Limited Max mode as shown in Table 1.