The following table describes the attributes used by the Cooling Proportional Valve with Dehumidification modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
CLG-OUTSTATE (State) |
G, V |
Current operational state of the output controller. |
Off Set Name: AHU Clg Valve Out |
|
Compensator Clg Cmd |
Controls the cooling valve. The valve is commanded from 0% to 100%. This output incorporates the Lead Compensator. |
0.0 Display Units: % |
|
|
Cooling Control Status |
V |
Contains the current saturation status of the controller. |
Normal Set Name: Control Status |
|
Cooling Percent Cmd |
V |
Controls the cooling valve. The valve is commanded from 0% to 100%. |
0% |
|
Dehum Process ID |
Specifies the type of process that this output controller is controlling when the mode is H Control:
|
RA-H Set Name: Process ID |
|
|
Failsoft Value |
Specifies the output when the mode is set to Failsoft. |
100% |
|
|
Flush Position |
Specifies the output when the mode is set to Water Flush. |
100% |
|
|
Humidity Process Variable |
Value of the relative humidity being measured by the humidity sensor. It is used as the process variable in the dehumidification control. |
50% RH |
|
|
Humidity Setpoint |
Contains the dehumidification Setpoint. |
50% RH |
|
|
Limited Max Value |
Specifies the output when the mode is set to Limited Max. |
100% |
|
|
Low OA Temperature Diff |
Indicates the differential for the Low OA Temperature mode. Once the valve is opened to allow water to flow through the coil during low OA temperature conditions, the OA temperature must increase above the OA Temperature Setpoint by the Low OA Temperature Diff before the valve can close. |
0.5 °C, 1 °F |
|
|
Low OA Temperature Position |
Specifies the output when the mode is set to Low OA Temperature. |
100% |
|
|
Low OA Temperature Setpoint |
Indicates the setpoint for the Low OA Temperature mode. When the OA Temperature falls below this setpoint, the valve opens. |
4 °C, 40 °F |
|
|
Mode |
Mode requested by State Selection. |
Off Set Name: AHU Clg Valve Out |
|
|
OA Temperature |
Indicates the Outside Air Temperature. |
4 °C, 40 °F |
|
|
Output Overridden |
Indicates when the actual output that is controlled by this output controller is overridden by a user. |
False |
|
|
Output Position |
Provides the current Present Value of the output that this controller drives. |
0% |
|
|
PID Tuning Reset |
Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID. |
Normal Set Name: PID Tuning Reset |
|
|
Process ID |
Specifies the type of process that this output controller is controlling when the mode is T Control:
|
DA-T Set Name: Process ID |
|
|
Process Units |
Specifies the units for the PID. For this particular module, °C and °F are the only two valid values. |
°C, °F Set Name: Unit |
|
|
Process Variable |
Specifies that when the mode is set to Control, this is the variable that is controlled. This value typically is connected to the Zone Temperature. |
13 °C, 55 °F |
|
|
Pump OnOff |
V |
Controls the circulating pump. |
Off Set Name: Off/On |
|
Setpoint |
Desired setpoint for the process variable to be controlled to when the mode is set to Control. |
13 °C, 55 °F |