Module Use in Applications (Cooling Proportional Valve) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names the following table.

Table 1. Cooling Proportional Valve Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Cooling Control v51

Fan Coil Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.