Primary States (Fan VAV Series) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Off: Turn the fan off. The Percent Cmd is set to 0% and the Fan OnOff is set to Off.

  • On: Turn the fan on at the Speed Setting value.

  • Hold: Hold the existing output.