Fan Three Speed - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module controls a three-speed fan. The module accepts a single input mode and produces three separate output On/Off commands. As the fan stages up, the module turns off the lower speed output first before turning on the higher speed output (following a very short delay so that both contacts are not closed at the same time). As the fan stages down, the module provides a user defined delay after turning off the higher speed output before turning on the lower speed output.

For information on how the FSM determines the state, see FSM (Three Speed Motor).

You can view and modify the modules in this group’s logic.