The following table describes the attributes used by the Fan Proportional modules.
|
Name |
Type cku1558008196875.html#cku1558008196875__cconfiguration_mode_gdefault |
Description |
Default Value |
|---|---|---|---|
|
Cooling Percent Cmd |
Contains the percent cooling, typically connected from the cooling output module. This value is used to span to a fan speed. |
||
|
Fan OnOff |
Contains the output command enumeration for information feedback representing the on/off status of the fan. |
Set Name: Off/On |
|
|
FAN-OUTSTATE (State) |
Current operational state of the output controller. |
Set Name: Off/On/Max |
|
|
Heating Percent Cmd |
Contains the percent cooling, typically connected from the heating output module. Used to span to a fan speed. |
||
|
Max Speed Cooling |
Contains the output percentage when the Cooling Percent Cmd input is at 100%. |
100.0% |
|
|
Max Speed Heating |
Contains the output percentage when the Heating Percent Cmd input is at 100%. |
100.0% |
|
|
Minimum Speed |
Specifies that when commanded to on, this is the minimum value that is output in the Percent Cmd output. |
20.0% |
|
|
Mode |
Mode requested by State Selection. |
Off Set Name: Off/On/Max |
|
|
Percent Cmd |
Output for fan control (0-100%). |
Display Units: % |