Attributes (Fan Supply Duct Static Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Fan Supply Duct Static Control modules.

Table 1. Fan Supply Duct Static Control Attributes

Name

Type akw1558008203339.html#akw1558008203339__fn13

Description

Default Value

Duct Static Pressure

 

Supply air duct static pressure.

250 Pa, 1 in. W.C.

Duct Static Pressure Setpoint

 

Normal supply air duct static pressure setpoint.

250 Pa, 1 in. W.C.

Emergency Duct Static Setpoint

 

Contains the supply air duct static pressure setpoint when Emergency S-P control is activated.

374 Pa, 1.5 in. W.C.

FSCS SF Cmd

 

Accepts a command from the FSCS and allows emergency response personnel to control the supply fan. Possible states are Auto, Off, and On.

Auto

Set Name: Auto/Off/On

Mode

 

Desired mode of operation.

Off

Set Name: AHU SF Control

Process Units

 

Specifies the units for the PID. For this particular module, Pa, in. W.C., Psi, and kPa are valid values.

Pa, in. W.C.

Set Name: Unit

Ramp Rate

 

Defines the rate of change in fan speed. This input is used in the Ramp mode.

50 Change per Minute

SF-OUTSTATE (State)

V, G

Indicates the current operational mode of the output controller.

Off

Set Name: AHU SF State

Supply Fan Control Status

V

PID Status. The possible values are Normal, Overridden, Disabled, Low, Timing Low, High, and Timing High.

Normal

Set Name: Control Status;

Supply Fan OnOff

V

Contains the control signal for the supply fan. The enumeration set only has two values, Off and On.

Off

Set Name: Off/On

Supply Fan Percent Cmd

V

Analog signal for the supply fan and uses it to command a fan speed. This output ranges from 0% to 100%.

0.0%

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)