Fan Supply Duct Static Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module is designed to use the supply fan to control the supply air duct static pressure. The module has inputs for the desired mode, a ramp rate, pressure, pressure setpoint, and process units. The module is also designed to accept commands from a FSCS. The FSCS input takes precedence over the mode input.