The following table describes the attributes used by the Fan Single Speed modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Fan OnOff |
Contains the output command enumeration for information feedback representing the on/off status of the fan. |
Set Name: Off/On |
|
|
FAN-OUTSTATE (State) |
Current operational state of the output controller. |
Set Name: Off/On/Hold |
|
|
Mode |
Mode requested by State Selection. |
Off Set Name: Off/On/Hold |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)