Fan Single Speed - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module controls a 2 position fan. The module accepts a mode input and it has an output to turn the fan on or off.

You can view and modify the modules in this group’s logic.