Fan Return or Exhaust BSP Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Return Fan BSP module controls a variable speed fan and building static pressure (BSP) in an air handler application. This module accepts building static pressure, and setpoints. The module has outputs for controlling a variable speed return fan.