Device OR - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module is responsible for examining two enumeration inputs and provides OR logic where at least one input must be On for the output to be On. The module accepts two Off/On inputs and has a output.