Feedback of Percent Cmd to UV Zone Damper Limit Control - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Zone Damper Limit Control uses the feedback of the Percent Cmd to begin controlling at the current damper position, when either form of limit control is required to maintain the discharge air temperature. When the transition out of a limit control occurs, the UV Zone Damper Control is already in control or the state requested is a fixed position state and does not require the Percent Cmd as its startup value.