Module Use in Applications (Damper Control [VAV Supply]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Damper Control (VAV Supply) Uses in Application System Selection Trees

Module Instance Name

Applications

CD Constant Damper Control v51

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

CD Damper Control v51

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

HD Constant Damper Control v51

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

HD Damper Control v51

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

Supply Damper Control v51

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.