Reliability (Min OA Fan Variable Capacity Flow Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

If the low limit process variable is unreliable, the damper closes and the fan de-energizes unless commanded to Emergency Open.

If the flow sensor is unreliable, module commands the fan off and the damper closed or it commands the fan on and the damper open based on a user selection.

All other inputs use their last reliable value while unreliable.