The following table describes the attributes used by the Min OA Damper 2 Position modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
COM Damper Control State (State) |
Represents the current module mode of operation. |
Close |
|
|
Damper Control Status |
Indicates current status of the controller for damper control. |
Normal Set Name: Control Status |
|
|
Differential |
Indicates the process type represented by the Process Variable. |
0 l/s, 0 cfm |
|
|
Min Air Flow Setpoint |
Indicates the analog percent output used to control the single actuator modulating the OA damper. |
0% |
|
|
Min Pos Low Setpoint |
When the Mode is Control Econ, this variable is controlled. For the Heat Pump this is typically Discharge Air Temperature. For the Unit Ventilator this is typically the Zone Temperature. |
10% |
|
|
Minimum OA Flow |
When the Mode is Control Econ, this variable is controlled. For the Heat Pump this is typically Zone Temperature. For the Unit Ventilator this is typically the Mixed Air Temperature. |
0 l/s, 0 cfm |
|
|
Minimum OA Flow Range |
Indicates the desired setpoint for the process variable to be controlled when the mode is Control Mode. |
0 l/s, 0 cfm |
|
|
Minimum OA Flow Setpoint |
Indicates the Mixed Air Temperature setpoint for Unit Ventilator and Zone Temperature Differential |
0 l/s, 0 cfm |
|
|
Mode |
Indicates the desired state. |
||
|
Output Overridden |
Indicates when the actual output controlled by this output is overridden by a user. |
False |
|
|
Output Position |
Provides the current Present Value of the output that this controller drives. |
0% |
|
|
PID Tuning Reset |
Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID. |
Normal Set Name: PID Tuning Reset |
|
|
Process Units |
Specifies the units for the cooling PID. For this particular module, °C and °F are the only two valid values. |
Set Name: UNIT |