The following table describes the attributes used by the Tower Control modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Command |
Starts the Fan OnOff 1 when in a Mode of On. |
False |
|
|
Delay |
Indicates the time in seconds to wait before turning on the Command output in Control Mode. This attribute is used to allow interlocked devices to activate before starting a primary device. |
5 Seconds |
|
|
Device OnOff |
G |
Provides a binary output to the primary controlled device and indicates whether any fan output is on. |
Off Set Name: Off/On |
|
Device OnOff 1 |
Provides a binary output to the primary controlled device and is used to start the Single or Low Speed Tower Fan. |
Off Set Name: Off/On |
|
|
Device OnOff 2 |
Provides a binary output to the primary controlled device and is used to start the Medium Speed Tower Fan. |
Off Set Name: Off/On |
|
|
Device OnOff 3 |
Provides a binary output to the primary controlled device and is used to start the High Speed Tower Fan. |
Off Set Name: Off/On |
|
|
Maintenance Switch |
Provides a binary input to disable or enable the controlled device. |
Enable Set Name: Disable Enable |
|
|
Mode |
Indicates the device’s mode of operation. |
Off Set Name: Off/On |
|
|
Output (Float) |
V |
Provides an analog output for the primary device and is used to modulate the boiler burner and load chiller, for example. |
0.0% |
|
Percent Cmd |
Provides an analog value input to determine the percent operating level of the controlled device. |
0.0% |
|
|
Percent Limit |
Provides a maximum analog output value for the controlled device and is used to limit the operation of an analog device. |
100% |
|
|
Ramp Time |
Indicates the time in minutes the ramp block takes to change from 0 to 100% output. |
1 Minute |
|
|
Rotate Enable |
Provides a binary output that determines whether the current device is allowed to run. |
False |
|
|
Safety |
Provides a binary input from an additional optional safety device (flow switch). This attribute is used to prevent a primary device from starting unless the safety is On when connected. |
On Set Name: Off/On |
|
|
Speed 2 |
Starts the Fan OnOff 2 when in a Mode of On. |
False |
|
|
Speed 3 |
Starts the Fan OnOff 3 when in a Mode of On. |
False |
|
|
State |
V |
Provide an Enum Output to indicate the operating mode of the module. |
Off Set Name: Off Low Med Hi |