Reliability (Rotation Small) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The reliability associated with the Sequencer module may report the input unreliable. When the input is unreliable, all outputs hold the last value set when the input was reliable.

If the Sequencer is unable to stage up or down because the remaining outputs are disabled, the Sequencer’s reliability is Unreliable.

The Sequencer module provides the following reliability values: Input unreliable, Unreliable.

This module does not associate any output with the module’s reliability. Therefore, even though the Reliability may not be equal to Reliable, the outputs from this module always appear Reliable.