Primary States (Rotation Small) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Idle: Idle State, Satisfied has no change pending.

  • Deactivated, Instant Shutdown: Instant Shutdown is True, shutdown is complete, all outputs are commanded off, and the input value is not being used to determine the number of required stages.

  • Shutdown In-Process: Instant Shutdown is True with a shutdown in progress.

  • Staging Up, Interstage On Delay: Needs to stage up and is waiting for Interstage On Delay to expire.

  • Staging Up, Minimum Off Delay: Needs to stage up and is waiting for Minimum Off Delay to expire.

  • Staging Down, Interstage Off Delay: Needs to Stage down and is waiting for Interstage Off Delay to expire.

  • Staging Down, Minimum On Delay: Needs to stage down and is waiting for Minimum On Delay to expire.