Attributes (Pump Startup Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Pump Startup Determination modules:

Table 1. Pump Startup Determination Attributes

Attribute

Type 1

Description

Default Value

Device nn Status

 

Indicates whether any of the pumps should be turned on. This module has 8 inputs.

False

Output

G

Indicates that one or more pumps should start. The output is an Or function of the inputs.

False

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)