Attributes (Pump Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Pump Control modules:

Table 1. Pump Control Attributes

Name

Type 1

Description

Default Value

Command

 

Starts or stops the pump when in a Mode of Control or Interlock Only.

False

Maintenance Switch

 

Provides a binary input to disable or enable the controlled device.

Enable

Set Name: Disable/Enable

Mode

 

Determines the operating mode of the module.

Off

Set Name: Plant Control

Off Delay

 

Indicates the time in seconds to wait before turning off the Device OnOff output in Control Mode. This attribute is used to allow interlocked devices to deactivate before stopping the primary device.

300 Seconds

On Delay

 

Indicates the time in seconds to wait before turning on the Device OnOff output in Control Mode. This attribute is used to allow interlocked devices to activate before starting the primary device.

20 Seconds

Output (Float)

V

Provides an analog output for the primary device. This attribute is used to modulate variable speed pumps.

0.0%

Percent Cmd

 

Provides an analog value input to determine the percent operating level of the controlled device.

0.0%

Percent Limit

 

Provides a maximum analog output value for the controlled device. This attribute is used to limit the operation of the analog device.

100%

PHWP1-OUTSTATE, SHWP1-OUTSTATE, CWP1-OUTSTATE, PCHWP1-OUTSTATE, OR SCHWP1-OUTSTATE (Device OnOff)

G

Provides a binary output to the primary controlled device. This attribute is used to start the pump.

Off

Set Name: Off/On

Ramp Time

 

Indicates the time in minutes that the ramp block takes to change from 0 to 100% output.

1 Minute

Rotate Enable

 

Provides a binary output that indicates whether the current device is allowed to run.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)