Primary States (Plant Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Off: Turns the device off. The Output is set to 0%, the Alarm is set to Off, the interlock Command is delayed off, and the Command is set to Off.

  • Control: Enables the Command Input to start and stop the interlock and the device.

  • Instant Shutdown: Turns the device off immediately. The Output is set to 0%, the Alarm is set to Off, the interlock Command is off, and the Command is set to Off. This state is used for Emergency Shutdown only and bypasses all timers which may cause dangerous conditions.

  • Interlock Only: Enables the Command Input to start and stop the interlock.