The application System Selection trees use the module names in the following table.
| Module Instance Name | Applications |
|---|---|
| Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
| EA Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
| OA Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
To see a module's connections and how modules interact with it, view the Connections table.