The following table describes the attributes used by this module.
| Attribute | Type 1 | Description | Default Value |
|---|---|---|---|
| Device 1 Cmd | Represents the command being sent to the first device. | Close | |
| Device 2 Cmd | Represents the command being sent to the second device. | Close | |
| Present Value | Represents the result of the OR operation. | Close |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)