Attributes (Cooling Tower Speed Count Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Cooling Tower Speed Count Determination modules:

Name

Type

Description

Default Value

Fan Type

 

Indicates the type of fans controlled by the central cooling plant. This module supports variable speed fans, 1-speed fans, 2-speed fans, 3-speed fans, and vernier control.

One Speed

Number of Towers

 

Indicates the number of cooling towers in the central plant.

3

Percent Cmd

 

Indicates the number of fans and at which speed they operate.

0%

Speed 1 Count

 

Indicates the number of fans at low speed.

0

Speed 2 Count

 

Indicates the number of fans at medium speed.

0

Speed 3 Count

 

Indicates the number of fans at high speed.

0