Fan Start Point Table (Cooling Tower Control) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This table is provided for reference only. The table indicates the start points for each tower and for each speed based on the number of towers and the number of speeds. The actual on/off request for each speed is generated by a sequencer external to this module. These requests are passed in via the Speed n Cmd, where n is 1, 2, or 3.

Figure 1. Fan Start Point Table