The following table describes the attributes used by the Subordinate Supply Flow Setpoint Control HFR modules.
|
Name |
Description |
Default Value |
|---|---|---|
|
Cooling Max Flow |
Contains the desired setpoint for the flow to be controlled when the cooling mode is set to Max Cooling. This is also the maximum flow when the mode is set to Control Cooling. |
500 l/s, 1000 cfm |
|
Cooling Min Flow |
Contains the desired setpoint for the flow to be controlled when the mode is set to Min Cooling. This is also the minimum flow when the mode is set to Control Cooling. |
0 l/s, 0 cfm |
|
Flow Percent |
Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow (whether heating or cooling) and 100% maps to max flow (whether heating or cooling). |
Display Units: % |
|
Flow Setpoint |
Contains the desired Flow Setpoint. This is the setpoint for another activity, typically the hybrid PVDC module. |
0 l/s, 0 cfm |
|
Heating Max Flow |
Maximum box flow setpoint used in Heating Flow Reset mode. |
250 l/s, 500 cfm |
|
Heating Min Flow |
Minimum flow setpoint under any heating conditions (that is, Heating or Warmup). |
0 l/s, 0 cfm |
|
Mode |
Mode requested by State Selection. |
Set Name: VAV Cascaded Flow Controller HFR
Default Value = Min |
|
State |
Contains the current operational state of the output controller. |
Set Name: VAV Cascaded Flow Controller HFR
Default Value = Min |