Module Use in Applications (Subordinate Supply Flow Setpoint Control Dual Duct) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Subordinate Supply Flow Setpoint Control Dual Duct Uses in Application System Selection Trees

Module Instance Name

Applications

Subordinate CD Constant Flow Setpoint Control

VAV Subordinate Dual Duct Applications

Subordinate CD Flow Setpoint Control

VAV Subordinate Dual Duct Applications

Subordinate HD Flow Setpoint Control

VAV Subordinate Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.