The following table describes the attributes used by the Subordinate Supply Flow Setpoint Control Dual Duct modules.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
CD Percent |
V |
Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow. |
0.0% |
|
CDFLOW-OUTSTATE, HDFLOW-OUTSTATE, or SAFLOW-OUTSTATE (State) |
G, V |
Current operational state of the output controller. |
Min Set Name: VAV DD Flow Controller |
|
Deck Max Flow |
Contains the maximum deck flow setpoint. |
500 l/s, 1000 cfm |
|
|
Deck Min Flow |
Contains the minimum deck flow setpoint. |
0 l/s, 0 cfm |
|
|
Flow Percent |
V |
Flow setpoint rescaled between 0 and 100 percent. 0% maps to the min flow and 100% maps to max flow. |
0.0% |
|
Flow Setpoint |
V |
Contains the desired flow setpoint. This is the setpoint for another activity, typically the Supply Damper Control module. |
0 l/s, 0 cfm |
|
Mode |
Contains the mode requested by State Selection. |
Off Set Name: VAV DD Flow Controller |